STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

unwind stack STM32H7 Free RTOS

HiI would like to store the call stack when the STM32H7 crashes. I implemented unwind.hThe code works on a bare metal  simple est code but not with   FreeRTOS is runningAny idea as to why?  The code  static uint16_t CallStackAddr;CALLSTACK_DATA uint3...

DCorn_0-1720086462291.png
DCorn by Associate III
  • 1466 Views
  • 1 replies
  • 0 kudos

Using STLink-V3SET in mass production

We are using STM32CubeProgrammer and STLINK-V3SET to program our products on our assembly line for mass production. We have a couple of questions 1) Is there a way to program using the command line or some other mechanism to keep a record of the numb...

STM32 UART Receive Problem

Hi, I am using STM 32 STLINK-V3. Thereis a problem with following UART receiver function.    __HAL_UART_CLEAR_FLAG(&huart5, UART_CLEAR_NEF|UART_CLEAR_OREF); HAL_UART_Receive(&huart5, rx_buffer, ROVER_MSG_LEN, 1000); __HAL_UART_DISABLE_IT(&hua...

Kuttay by Associate III
  • 11242 Views
  • 12 replies
  • 4 kudos

Stat and stop toggle of output compare mode precisely

Hi all,  for a projet I need to create a signal at 500khz, and every 60 µs I want to stop the toggle (or not) I generate the signal with the output compare of tim2 (on stm32L073)then, in TIM2_IRQHandler(void)I try to count the number of call, then st...

Seth1er by Associate II
  • 1925 Views
  • 3 replies
  • 0 kudos

Vss pin setting

Hi. I'm using STM32F303RCT6 now. Is it possible to set one pin vss using gpio settings? If so, is there a specific pin? If you have any question, ask me.Thank you. 

giwonKIM by Associate III
  • 2807 Views
  • 6 replies
  • 0 kudos

STlink v2 live debugger does not capture COM port

Hi,I have written application using visual studio C#. And I send commands through the COM port from my Visual Studio application to my STM32 board. There is a bit of strangeness, when I run the live debugger using STlink V2 with STM32CubeIDE I can se...

cjaya.2 by Associate II
  • 1178 Views
  • 1 replies
  • 1 kudos

I2C issue when called from external file

Hi There, We have IO expander that is connected using I2CFile: Application.C has functions for change the IO value of the IO Expanderthere is a UART that the user can connect to and change the value of the IO Expander (using CLI) Following functions ...

GalBTM_0-1719310004297.png
GalBTM by Associate II
  • 2283 Views
  • 4 replies
  • 0 kudos