User Activity

Sorry, are there has a pin call or used for SD_detect in Stm32l431rct6? I can not find in STM32L431xx Datasheet - production data. These has no mention.I do not know which pin(SD-Detect)should i choose for GPIO_Input of the FATS.
I am following the tutorial from https://www.youtube.com/watch?v=I9KDN1o6924&t=384s the tutorial(32F746GDISCOVERY) User manual has showed MicroSDcard_detect is pin PC13.I can not find my pin name of stm32l431rct6 Datasheet for MicroSDcard_detect pin....
I start the project(SDIO+FATFS)from the .ioc file and also regenerate the project from CubeMX with IDE as a toolchain and unchecking the "Generate under root". But after i generated, the project does not have anything. 
Kudos given to