STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F373 SADC how to get 0-3.3V 16 bit(65535)?

Hello Friends,I use STM32F373 for 16-bit SADC.I have single-ended input 0V to 3.3V. VREFSD+=3.3V and VREFSD- =0VWhen input Voltage change from 0V to 3.3V I get values 0 to 32767. Is it not possible to get 16-bit (65535) data?Always signed?my configur...

Resolved! stm32g0b1 dual flash bank address ambiguity

Hii have STM32G0B1KEi was configuring the cube-eeprom-v7 emulation to use the last two pages from bank2 to store some configuration.when i came to set `START_PAGE_ADDRESS` i need the address of the second last page.reading in the 'Table 11. Flash mem...

Screenshot from 2024-07-30 08-24-28.png
encoder by Associate
  • 1540 Views
  • 1 replies
  • 0 kudos

Resolved! STM32h757 base custom board not detected.

Greetings,I have just received my custom made STM32H757 based boards, when I try to connect with it using the USB cable its not detected at all in my windows 10 PC but I am able to connect with it in DFU mode or using the stlink-V2 through SWD.This i...

Resolved! IO2 QSPI pin

While using the Quad SPI mode of the OCTOSPI peripheral for four lanes, it was observed that when used in input mode all the pins except IO2 function properly. We can see the signal coming to the pin when probed externally, but it just does not seem ...

AShetty by Associate II
  • 2071 Views
  • 3 replies
  • 1 kudos

Resolved! SPI DMA Doesn't work in Nucleo-STM32u575ZITxQ

Hello ,  I have an issue in STM32u575 IN SPI DMA , Even IF I Tried the Example code (/SPI_FullDuplex_ComDMA_Master)  there is no data received from the other side  iam using the aardvark to test it  when check the return of this function  HAL_SPI_Get...

dynamic address broadcast not working for Nulceo-H563ZI

I just downloaded the "I3C_Controller_WakeUpFromStop" project for the Nucleo-H563ZI board using the example project import option. It compiled with no issues. Ran it with debugger and protocol analyzer on the I3C bus. When the subroutine "Handle_ENTD...

JRM_02 by Associate II
  • 1523 Views
  • 1 replies
  • 0 kudos

STM32H5 I3C SETGRPA

Hello !I am using the I3C interface between a STM32H563ZI and 2 LPS28 sensors. After a ENTDAA process I would like to send a SETGRPA but unfortunately it does not work. It seems the process fails during HAL_I3C_AddDescToFrame() due probably to a wron...

Capture d’écran 2024-07-17 à 16.35.13.png
Phil91 by Associate
  • 1390 Views
  • 1 replies
  • 0 kudos