STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Modification/Clarification of Chirp Signal Code

Hello, first of all, I hope im at the right section for my question. If not I'm sorry.I'm relativ new in working with Nucleo Boards and currently working on a Project where i want to generate a chirp signal/sinus sweep from -20kHz up to 20kHz.I made ...

Screenshot 2024-08-01 133717.png Screenshot 2024-08-01 133819.png

Resolved! LwIP integration with external PHY

Hello, is it possible to ușe the LwIP Middleware over the low level library for an external PHY such as ENC28J60?If so, could you pinpoint me to a documentation or an article?Thanks.

TheoMj by Associate
  • 2664 Views
  • 1 replies
  • 1 kudos

DAC underrun when writing to a HRTIM register

Hi,I have the following configuration:1. ADC converts values and writes it to memory with DMA2. DAC outputs the ADC data also with a DMA3. Both, the ADC and the DAC are triggered by HRTIM TimerA at a rate of 700kHzAll works fine, I can see the data c...

berait by Associate III
  • 1069 Views
  • 1 replies
  • 0 kudos

Resolved! VBAT & RTC Issues on Circuit - STM32H563ZIT6

I am experiencing issues with the VBAT pin on the STM32H563ZIT6 microcontroller. Specifically, the VBAT pin is not responding properly. I am using a CR2032 CMOS battery for RTC backup, but it is not maintaining the date and time as expected. When the...

VBAT_CKT.png CMOS Battery.png

STM32L053 I2C problems with LIS3DH sensor

Hi, I'm trying to recover the data from the LIS3DH sensor and I found this tutorial " https://www.youtube.com/watch?v=A1CIOUZdeR4". In the tutorial the person uses function " if(HAL_I2C_IsDeviceReady(&hi2c1,SLAVEI2C_ADD,10,100)==HAL_OK) " to see if t...

0690X000006DavhQAC.png
JJavi by Associate II
  • 6278 Views
  • 11 replies
  • 0 kudos