STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

driver for external SRAM chip - IS66WVS4M8ALL/BLL

Hi, I'm trying to add an external memory and i choose that chip because it can communicate with QSPI and there is no need for designing due the chip is SOIC-8 which i found a compatible board for it. I'm getting issues with the driver writing i'm get...

Ditzhak_0-1722495083492.png
Ditzhak by Associate III
  • 3221 Views
  • 5 replies
  • 2 kudos

Nucleo-L4P5ZG LPUART not receiving nor transmitting

Hi all! I am trying to communicate with the Nucleo-L4P5ZG via the LPUART1 peripheral over ST-LINK, however it doesn't seem to be transmitting or receiving anything. Following is my system clock initialization code (non-relevant parts cut out): #pragm...

CubeIDE and c++ routines problems

Hi to all,I am moving to SPM32CubeIDE on Linux and, as a newby, I encountered a lot of problems.I started a new empty C++ project and I put all my flies and classes.I also included syscall.c file (renamed in syscall.cpp) as in it there are _seek(), _...

Resolved! STM32F446VET7 LoRa E220-400T30S UART Communication

Hello,I am trying write a LoRa library to STM32F446VET7 in my application.In the LoRa E220-400T30S documentation, it tells me to set the UART settings for configuration mode to 9600 and 8N1 and to give 1 to M0 - M1 pins.After doing that I am trying a...

testbenchmark_0-1722677845691.png testbenchmark_1-1722678016431.png testbenchmark_2-1722678063835.png testbenchmark_3-1722678118028.png

Resolved! FT812, Correct way to manually configure SPI?

Hi guys, I'm fairly a newbie to stm32 so please forgive me if I make some mistakes, I'm trying to configure a driver code for a SPI FT812 NHD display on STM32G474VETx chipset, so far I've been able find a driver code and ported it over onto STM32, ho...

Resolved! Short read from multiple ADCs under DMA

Using a stm32f303RE Nucleo board which has 4 (independent ?) ADC blocks.I'm trying to read a single channel from each of the 4 ADC under DMA simultaneously triggered from the same timer update event but I'm only getting about 30-40% of the data I'm a...

Resolved! STM32G491RE MCU getting struck

Hi,I am working on stm32g491re custom board.I am using STM32cubeide  and segger jlink debugger with serial wire debug.After flashing the firmware program getting struct at intializationlike HAL_GPIO_INIT()and HAL_TIMER_init()if I try to suspend the r...

STM32H725 temperature sensors

Hello, I am trying to measure Junction temperature of the STM32H725IG device.ADC3 is configured as an errata say to have only temperature channel 17 and continuous measurement. Temperature I see seems to be between 60 and 80 degree Celsius.I tried al...