STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB DFU Mode in STM32G0

Hi all, per AN3156 it states G0 series have USB DFU mode built-in the factory bootloader, so does it mean I won't have to configure the USB Device DFU Class in the CubeMX in order to make it work? Could I configure it into other classes (like CDC Vir...

TSu.1 by Associate III
  • 1811 Views
  • 1 replies
  • 1 kudos

Rewrite consecutive FLASH pages

Hello.I am creating a program to write data to multiple FLASH memories using the STM32C031.I have set FLASH page13,14,15 as new pages to be written, but only page13, which is the first page to be rewritten with FLASH, is rewritten, while page14 and 1...

shank by Associate III
  • 2054 Views
  • 3 replies
  • 1 kudos

Resolved! Cortex-M0 Vector table relocation.

To give a context:I'm working to implement OTA for an existing project which uses stm32f091xx.And it already contains separate bootloader(0x08000000) and application(0x08001000) with their own vector tables.Currently, when a reset occurs, the bootloa...

Vmere.1 by Senior
  • 5806 Views
  • 4 replies
  • 0 kudos

STM32H723 PSSI DE/RDY lines

Hi,Can anyone explain how DE/RDY lines are working in different directions? I am getting confused while reading the Ref manual. The RM0468 states in Table 305 the PSSI_DE is an Input which serves as " Data enable signal: data valid signal when receiv...

dsn by Associate
  • 1159 Views
  • 0 replies
  • 0 kudos

Resolved! STM32 // QFB09C1

Dear, My customer is looking for the STM32 MCU that can connect to wifi without using an antenna, has more than 33 GPIO (Digital Output) but not too many outputs and can operate stably in an industrial environment.Please advise the possible product. ...

Resolved! STM32H743II W25Q128 Custom External Loader Issues

hello friends!Now a days i started working on TouchGFX for Waveshare's OpenH7XXI-C board and CoreH7XXI MCU. I interfaced 7 inch display, FMC SDRAM as bank 2 and W25Q128 QSPI. after configuring these peripherals i tested them manually by writing and r...