Hi,I'm running STM32C011F4U6TR using the LSI (32KHz) in a infinite loop.Here's the current consumption I see from the STM32CubeMonitor-Power softwareI expect to see around 80uA flat as datasheet shows at page 39What could be the reason for the 170uA ...
Hi,If I configure the LSI as clock source my STM32C011F4U6TR code stuck at this pointHowever there is no problem if I configure HSISYS as clock source.Why? Could anyone help me with this issue?Thanks in advance,Gaston
Hi,I'm not able to set the STM32G030C6 ADC1 for 9 + Internal Temperature Sensor channels. Here's my ADC1 Mode and Configuration parameters I'm using this recently updated Software Package VersionSTM32CubeG0 Firmware Package V1.6.2Does anyone know wha...
Hi,I cannot understand acquired ADC data order using this configuration on a STM32G030C6 device:I want to acquire 9 input channels + 2 internal channels (Temperature Sensor + Vbat). Continuous mode w/ Circular DMAHere's my Initialization routine stat...
First let me thank you for posting and welcome to the ST Community.I am a member of the community since 2018 but thanks anyway.Before the selection of the STM32CubeIDE version, I suggest that you log to your ST account.It is irritating to download th...
Great! When will this problem be fixed?https://community.st.com/t5/stm32-mcus-products/stmg0-multichannel-adc-cubeide-configuration-issue/m-p/692956#M254052Gaston
No. It does not work with latest CubeIDE v1.16 (CubeMX v6.12) update.I've downgraded the iDE to v1.15.2 (CubeMX 6.11.1) and it works fine.It seems a CubeIDE v1.16 issue