STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMx Bugs - ADC, USART, NVIC

Posted on January 27, 2015 at 13:39STM32CubeMx v4.6.0 STM32F4 v1.4.0 1. After close and open CubeMx project (create for STM32F4DISCOVERY), i see ADC1 config error (in the previous version of the same here): 2. I set USART speed 57600, it work on 115...

0690X00000605SRQAY.png 0690X00000605fcQAA.png 0690X00000605b9QAA.png 0690X00000605HvQAI.png
levak by Associate II
  • 2685 Views
  • 5 replies
  • 0 kudos

Problem with STm32 discovery GPIO using HAL Driver

Posted on March 11, 2015 at 11:21 Hi I am new to Stm32 devices and am trying to get the discovery working for basic functions.I have followed the manual to set up and run the GPIO pins, But I donot seem to get it working. The examples pro...

STM32L151 MISO AF config issue

Posted on February 26, 2015 at 18:39Hi all, I'm using L1 series for the very first time. The code is generated with CubeMX 4.6.0 and built with MDK 5.12.0. I've had Cube MX copy the device library into the project directory. My board carries an STM3...

Alex Yang by Associate II
  • 1644 Views
  • 3 replies
  • 0 kudos

STM32CUBE Problem configuring MISO

Posted on March 09, 2015 at 19:27 CubeMx version: 4.6.0Target: STM32L152VBTxI configured SPI1 as a full duplex master.I put MISO on PE14Cube configured the GPIO as a standard input.It wouldn't let me set it to Alternate function.I was able to over...

STM32F334 How to deal with multiples ADC triggers?

Posted on September 15, 2014 at 17:26Hi,STM32F334 has a great HRTIM capable of driving up to 5 half bridge converters, but it has only 2 ADC that share the same interrupt, how to trigger the ADCs in 5 different points?Ari

Asantos by Senior
  • 1424 Views
  • 3 replies
  • 0 kudos

STM32L+microSD card

Posted on March 17, 2015 at 18:34Hi everyone, I'm working with stm32L152 discovery. I'd like to be able to create files on a microSD which contain data from a sensor and successively read these files from a PC. If I understand it, once I configured ...

simval986 by Associate II
  • 1179 Views
  • 2 replies
  • 0 kudos

STM32F334 and high-resolution timer

Posted on August 25, 2014 at 09:27New STM32F334 have high-resolution timer with 217 ps resolution, It's nice,butwhatrealprecision is achievedwhenthe timerused to measure thetimebetweentwo edgesof the signal appliedtothe processorGPIO?

a1379109 by Associate
  • 1085 Views
  • 1 replies
  • 0 kudos

Problem with Flash Loader Demostrator Version 2.7.0

Posted on March 12, 2015 at 19:42I am having a problem with Flash Loader Demonstrator Version 2.7.0. I am trying to program the FLASH of an STM32F427ZIT ARM processor using the USART3 serial port. I am running Flash Loader Demonstrator on an XP comp...

krubow by Associate II
  • 7774 Views
  • 1 replies
  • 0 kudos

STM32 with TSL2561 I2C

Posted on March 17, 2015 at 12:31Hi, I'm working on STM32F072b discovery board. I am new to this so I don't know much. I am trying to make the luminosity sensor, TSL2561 with I2C serial bus communicate with my dis.board. Can someone show me step b...

eeyjws by Associate II
  • 1435 Views
  • 2 replies
  • 0 kudos