cancel
Showing results for 
Search instead for 
Did you mean: 

sd card init problem

Tamas Novak
Associate III
Posted on January 02, 2015 at 14:28

My STM32F429 board uses Kingston 4GB uSDHC card. CubeF4v1.3.0 HAL init fails in

SD_PowerON() function in stm32f4xx_hal_sd.c

/* Send CMD55 */

  sdio_cmdinitstructure.Argument         = 0;

  sdio_cmdinitstructure.CmdIndex         = SD_CMD_APP_CMD;

  SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);

 

  /* Check for error conditions */

  errorstate = SD_CmdResp1Error(hsd, SD_CMD_APP_CMD);

 

  /* If errorstate is Command TimeOut, it is a MMC card */

  /* If errorstate is SD_OK it is a SD card: SD card 2.0 (voltage range mismatch)

     or SD card 1.x */

  if(errorstate == SD_OK)

  {

    /* SD CARD */

    /* Send ACMD41 SD_APP_OP_COND with Argument 0x80100000 */

    while((!validvoltage) && (count < SD_MAX_VOLT_TRIAL))

    {

      

      /* SEND CMD55 APP_CMD with RCA as 0 */

      sdio_cmdinitstructure.Argument         = 0;

      sdio_cmdinitstructure.CmdIndex         = SD_CMD_APP_CMD;

      sdio_cmdinitstructure.Response         = SDIO_RESPONSE_SHORT;

      sdio_cmdinitstructure.WaitForInterrupt = SDIO_WAIT_NO;

      sdio_cmdinitstructure.CPSM             = SDIO_CPSM_ENABLE;

      SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);

 

I check SD_CMD and SD_CLK with oscilloscope:

1) 400kHz clock starts,

2) CMD0 then CMD8 sent

3) 200usec no response

4) CMD55 send (payload 0)

5) response after 4 clk cycles:  0x 37 00 80 01 20  04

which is CMD55 response, CRC is x04

If I stop at the breakpoint (red line in code),

errorstate variable

contains 15: SD_COM_CRC_FAILED.

For me CRC 0000100 seems to be fine for that message, I don't know why ''errorstate'' fails, but init won't continue with AMCD41...

I've tried it with other 8GB Kingston microSD HD...same thing.

Any idea what can cause this?

#sd-card-init
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Tamas Novak
Associate III
Posted on January 04, 2015 at 11:46

To be exact, response sent by the SD card is 0x 37 00 80 01 20 

09

, where last byte is 0000100 7-bit CRC and ''1'' stop bit.

I calculated CRC by online calculator:

https://ghsi.de/CRC/index.php?Polynom=10001001&Message=37+00+80+01+20

Polynom is x7 + x3 + x0 for calculation.