STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32cubef4 ----- do examples work

Posted on March 19, 2015 at 08:24I'm new to STM32 so downloaded Keil V5 and stm32cubef4. Tried compiling the first example using the STM32F4-DISCOVERY. I got many errors so changed the include location in the project properties then compiled but got...

Problem with I2S interface: No clock on WS and SCK pins

Posted on March 13, 2015 at 10:47Hi I use a STM32L100C-DISCO kit. I want to use I2S interface. I configure this interface with STM32CubeMX: I enable I2S2 as Half Duplex Master, I choose HSI and internal clocks to have an audio clock of 48kHz. Every...

helene by Associate II
  • 2232 Views
  • 3 replies
  • 0 kudos

ST32F4 Systick_handler problem

Posted on March 18, 2015 at 16:34Hey,I am currently working on a project with an STM32F4 MCU. My board works fine until I try to put some output high and then a few seconds later low, this is done with starting a timer. After a couple of times for s...

T.Dieter by Associate
  • 921 Views
  • 1 replies
  • 0 kudos

STM32F4 RTC Problem

Posted on September 01, 2014 at 13:25I have a STM32F405RG with external 16MHz crystal which is also used, divided by 16 as the RTC clock source.  The project has been built using VisualGDB. The problem is that the RTC appears to stop after it is rea...

malcolm2 by Associate II
  • 2038 Views
  • 3 replies
  • 0 kudos

STM32 MCU

Posted on January 08, 2015 at 10:26Hi Guys,I am using the STM32F207VG development board.I'm having problem in compiling the example codes given by STM. Since there is no dedicated IDE for STM32 devices what is the recommended FREE IDE from STM? I ma...

I2C - IMU 6DOF

Posted on March 11, 2015 at 05:00Dear all, I am doing a project that control a quadcopter using STM32F103. At this moment, I have done about the control of DC motor. However, my quad. is not stable when it takes off. I am going to use IMU 6DOF ( ...

Using malloc

Posted on March 18, 2015 at 09:04HiI have a bit of a problem when using malloc so I was wondering what others think about this. I use malloc in my application, mainly because the application is entirely asynchronous so either I have to use malloc or...

per2399 by Associate II
  • 7733 Views
  • 3 replies
  • 0 kudos

IP Phone

Posted on February 08, 2015 at 19:29How to make IP-Phone?, Its Main question.I have some experiences on audio broadcasting with STM32 (UDP+RTP+[aLaw-uLaw]).I don`t know how to complete it to make a IP-Phone.I know SIP stack is needed too. but I don`...