display driver
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-01-03 7:18 AM
Posted on January 03, 2016 at 16:18
I have the nucleo board and an add-on board with a 2x12 oled character display. Writing to the display is not straight forward because D7..D0 lines are connected to pins on different ports (PA,PB,PC).
Is there a way to structure this hardware so I can write clean C code? For instance RS is PB3, WR is PC1, Enable is PA10, D7 is PA8, D6 is PB10, D5 is PB4, D4 is PB5, D3 is PA9, D2 is PC7, D1 is PA3, D0 is PA2. Thanks #port-pins
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-01-03 9:39 AM
Posted on January 03, 2016 at 18:39
Is there a way to structure this hardware so I can write clean C code?
Manage the data pin output in a single function so the complication is abstracted from all the other code?Either use a table driven method, bit mapping, or use a shift/masking technique for contiguous bits.GPIO_WriteBit(GPIOA, GPIO_Pin_2, (x & 1));GPIO_WriteBit(GPIOA, GPIO_Pin_3, (x & 2));...
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..