STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How transfer info from flash QSPI to SDRAM .

Posted on April 21, 2017 at 23:20HiI use STM32f779  and i have TFT LCD 800x480   controller tft is RA8875 .  I want to transfert my images to flash after i need to transfert to SDRAM  and transfert to controller RA8875 .   Can you help me how transf...

Resolved! Windows CDC Driver issue

Posted on September 02, 2016 at 08:34Hello.I want to use the USB High Speed with the class CDC in device mode. I am using the STM32F746G-DISCO board.I have created a project with STM32CubeMX , here there is the configuration : MiddleWare : USB DEVIC...

y23 by Associate
  • 3685 Views
  • 4 replies
  • 0 kudos

first time here - help with stlink programmer

Posted on April 22, 2017 at 00:54Hi there people!Ive got one big but a very basic question for yallIm just curious if following things are even possible and is this forum right place to find infoIve never ever been into this so know absolutely nothi...

MAC-layer of STM32F7

Posted on April 22, 2017 at 11:08Hi all,Problem with sending packet from MAC-layer of STM32F745VG to Physical Layer Transiver.ARP-packet is prepared to transfer after start. It is sent to Physical Layer Transiver in Evaluation Board (STM32746-EVAL2)...

what is the maximum FSMC_CLK value for STM32F2 series?

Posted on April 21, 2017 at 14:49Hi,I am trying to set freq for FSMC, I am using STM32CubeMX for code generation.In clock configuration segment which clock is related with FSMC(is it APB1 peripheral clocks???).Please find the attached image file for...

Sensor MPU6050 with stm32

Posted on April 21, 2017 at 18:29Sorry! I have module  MPU6050 and STM32F103C8T6. I want to use it to get data but I don't know to work with them.Help me! Thank all :( 

Stm32f030f4p6 POR current problem

Posted on April 19, 2017 at 16:26Hi,I have designed low power detector with using stm32f030f4p6. In normal state detector is supplied with 24Vdc and it consumes 50uA. But when I supply the detector with 2V, mcu consumes 2mA. This high current consum...

stm32f429 rotary encoder external interrupt

Posted on January 05, 2017 at 10:43Hi,I am using rotary encoder with two input i/o and i want to read the encoder pinA and pinB values with external interrupt. I am using callback function for two input PA0 and PA1. My functions are below:In stm32f4...

er3481 by Senior
  • 1750 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F4 Camera with STM32F7 Discovery board?

Posted on February 19, 2017 at 20:59Hi all,I'm trying to use the camera STM32F4DIS-CAM with my STM32F7 Discovery board, with Keil uVision IDE. I have downloaded STM32Cube, and in the examples there is a BSP directory, with BSP drivers examples, incl...