Skip to main content
benjaminbrammer9
Associate III
November 14, 2016
Question

STM32CubeMX Clock configuration error

  • November 14, 2016
  • 2 replies
  • 1132 views
Posted on November 14, 2016 at 16:59

Hi guys,

I want to use the internal 8MHz HSI reference for generating my clocks, but allthough there is now clock speed error to resolve I still get an error that the HSI is not recommended for the PLL as input. Why is that? And if this is the case, why does STM offer the possibility to do so?

here's an image of my clock configuration.

best regards

Benjamin

    This topic has been closed for replies.

    2 replies

    Jeanne Joly
    Associate
    November 15, 2016
    Posted on November 15, 2016 at 16:59

    Hi brammer.benjamin,

    In some application note on the clock configuration tool, you can find in the chapter clock scheme : 

    ''For accuracyreasons, the USB peripheral must only be driven by the PLL configured with theHSE clock source.''

    On the picture you shared, I can see that you activated USB and in this case, as written previously, only HSE clock source can be activated.

    I hope it is clearer.

    BR

    Eric Dampierre.

    benjaminbrammer9
    Associate III
    November 18, 2016
    Posted on November 18, 2016 at 10:01

    Thanks for your reply!

    Yes, now it is clear, so I will implement an external crystal.

    best regards

    Benjamin