cancel
Showing results for 
Search instead for 
Did you mean: 

ADC reading value

sbertuletti
Associate II
Posted on November 17, 2016 at 18:26

Why if i put a voltage equal to 1V to the ADC input of the microcontroller, i read a value equal to 1.4 V??

It seems that the Voltage_Actual_Value=0.7*ADC_Value

Thanks

#more-facts #!stm32-!adc #please.
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
AvaTar
Lead
Posted on November 18, 2016 at 09:26

>Why if i put a voltage equal to 1V to the ADC input of the microcontroller, i read a value equal to 1.4 V??

 

What makes you think so ?

slimen
Senior
Posted on November 18, 2016 at 09:30

Hello,

Which board are you using?

You may refer to your product datasheet or reference manual for more clarification.

Regards

sbertuletti
Associate II
Posted on November 18, 2016 at 09:36

I used different boards: STM32F411RE_NUCLEO, STM32F401RE_NUCLEO and STM32L071 microcontroller. 

AvaTar
Lead
Posted on November 18, 2016 at 10:48

> Which board are you using?

This is less a question of board(s) involved, but rather of missing knowledge at the O.P.'s side about the inner workings of an ADC.

ColdWeather
Senior
Posted on November 18, 2016 at 12:31

If you read an ADC value out, you read no voltage but some number between 0 and 4095 (for 12-bit ADC). The weight of the lowest bit depends on the reference voltage Vref used by the ADC. In the most cases that is the VCC - the supply voltage of the CPU. Mostly 3.3V, some Discovery boards have 3.0V. Thus, the actual voltage measured by the ADC is

V = Vref * ADC_Value / 4095

for the Vref = VCC = 3.3V:

V = 3.3 * ADC_Value / 4095

The VCC can vary. To solve this, you can use alternatively the internal voltage reference Vint = 1.2V to find the weight of the lowest ADC bit out. Measure the Vint by the ADC, you'll get some number ADC_Int:

Weight = Vint / ADC_Int = 1.2 / ADC_Int (volts per bit)

then the measured external voltage would be

V = Weight * ADC_Value = Vint * ADC_Value / ADC_Int

and the VCC used as the Vref:

VCC = 4095 * Weight = 4095 * Vint / ADC_Int = 4914 / ADC_Int .

Check this on your boards.

sbertuletti
Associate II
Posted on November 18, 2016 at 12:57

Thanks for the explanation. I'll check it on my board