User Activity

Posted on December 08, 2016 at 19:01 So I finally got my IL9325 TFT display running via FMC but it is running much slower than I expected. The SPI based displays on arduinos seem to be performing better than this parallel setup. I measured my data ...
Posted on November 18, 2016 at 16:39Hello,I am working with a smart TFT that supports the 8080 parallel interface on a custom board but the design omitted connecting the RD, RS, CS, WD to the appropriate NEx, NOE, NWE, Ax pins. Instead these 4 contr...
Posted on November 16, 2016 at 06:42Hello,I am trying to configure pins D0-D15 on the STM32F429VIT6 to output sram data. The code seems to be functioning properly and I have scoped out each of the pins however Pin44(PE13)-D10 seems to never go high....