Question
Disable RX TX Callbacks - Uart DMA stop
Posted on December 17, 2015 at 07:21
Hello there,
I am using uart tx and rx with dma. It works, but each time I stop the DMA using:/**
* @brief Stops the DMA Transfer.
* @param huart: pointer to a UART_HandleTypeDef structure that contains
* the configuration information for the specified UART module.
* @retval HAL status
*/
HAL_StatusTypeDef HAL_UART_DMAStop(UART_HandleTypeDef *huart)
{
/* The Lock is not implemented on this API to allow the user application
to call the HAL UART API under callbacks HAL_UART_TxCpltCallback() / HAL_UART_RxCpltCallback():
when calling HAL_DMA_Abort() API the DMA TX/RX Transfer complete interrupt is generated
and the correspond call back is executed HAL_UART_TxCpltCallback() / HAL_UART_RxCpltCallback()
*/
/* Disable the UART Tx/Rx DMA requests */
huart->Instance->CR3 &= ~USART_CR3_DMAT;
huart->Instance->CR3 &= ~USART_CR3_DMAR;
/* Abort the UART DMA tx Stream */
if(huart->hdmatx != NULL)
{
HAL_DMA_Abort(huart->hdmatx);
}
/* Abort the UART DMA rx Stream */
if(huart->hdmarx != NULL)
{
HAL_DMA_Abort(huart->hdmarx);
}
huart->State = HAL_UART_STATE_READY;
return HAL_OK;
}
The TxCpltCallback and RxCpltCallback interrupts are generated. What would I have to do to disable them, so they wont be generated when I stop DMA? I tried HAL_UART_DMAPause before or HAL_NVIC_DisableIRQ but that did not help.
I would really apreciate help.