STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PA0 and NUCLEO-H743ZI

Hello,I want to use TIM3 as 32-Bit counter. Clock source is set to ETR2. The corresponding Pin is PA0. For test purpose I use TIM3 to generate a clock signal (Pin PC6) to feed the TIM3 counter.Connecting these to pins together (PA0 and PC6) results i...

HAL_UART_Receive not working after a while!

Dear friends,there are two threads in my application , one is used for TCP/IP using lwIP and the other one is for RS485 protocol. Everything works fine correctly and I can send and receive data on RS485. After two or three hours or sometimes sooner, ...

Mujtaba by Senior
  • 785 Views
  • 1 replies
  • 0 kudos

Resolved! Where does the output of 'sprintf' goes to ?

Hello,I use stm32cubeH7 examples.I find in some of them call to sprintf, yet I don't understand where is the output of the sprintf goes to:I tried opening the "STMicroelectronics STLink virtual com port" - nothing is printed hereI also tried to searc...

ranran by Senior II
  • 1503 Views
  • 3 replies
  • 0 kudos

CAN Setup with STM32-Mat/Target in Simulink ?

Hello,I'm trying to use the STM32 MAT/TARGET to setup a Communication between Simulink and a STM32f107vct via CAN.When I want to build the Simulink model i get an "INVALID INDEX" Block Diagram error.I am using Matlab R2018b and the latest version of ...

JVier by Associate
  • 1285 Views
  • 1 replies
  • 2 kudos

STM32F103 UART Tx interrupt

Posted on February 07, 2015 at 13:30Hell all, I have two UARTS connected to two devices (say A and B). Both UARTs Tx and Rx is interrupt based. When I receive a message from A (ASCII-Z string) and the same message is sent to B, I am getting the mess...

nps by Associate II
  • 3446 Views
  • 2 replies
  • 0 kudos

Sending UART data at maximum speed without interrupts

Hi,There something odd with the USART3 (the Virtual COM one). I can send characters, but there's some speed limit that I can't surpass.I'm trying to loop a string as fast as possible, but I can't get the optimum speed, I'm having to use a delay (or a...

Resolved! NVIC_Init() library function does not work as expected

Hi All, I have simple code to assign preemption priority and subpriority. I have tested this code on the stm32f103. Even if i set the preemption priority and subpriority, when I read the priority it returns as 0x00. According to the information from ...

ebast by Associate II
  • 2203 Views
  • 2 replies
  • 0 kudos