cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f429 freertos fatfs with sdio and dma

li jinqiu
Associate II
Posted on September 09, 2017 at 13:11

I use the cubemx to create the project(cubemx 4.22 and stm32CubeF4 1.16),it always occurs FIFO Error Interrupt,when I use dma to write sdio. And It stopes.,when write serveral times.But there is no sdio error interrupt happened.

This is my dma configtion:

/* SDIO DMA Init */

/* SDIO_RX Init */

hdma_sdio_rx.Instance = DMA2_Stream3;

hdma_sdio_rx.Init.Channel = DMA_CHANNEL_4;

hdma_sdio_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;

hdma_sdio_rx.Init.PeriphInc = DMA_PINC_DISABLE;

hdma_sdio_rx.Init.MemInc = DMA_MINC_ENABLE;

hdma_sdio_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;

hdma_sdio_rx.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;

hdma_sdio_rx.Init.Mode = DMA_PFCTRL;

hdma_sdio_rx.Init.Priority = DMA_PRIORITY_VERY_HIGH;

hdma_sdio_rx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;

hdma_sdio_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;

hdma_sdio_rx.Init.MemBurst = DMA_MBURST_INC4;

hdma_sdio_rx.Init.PeriphBurst = DMA_PBURST_INC4;

if (HAL_DMA_Init(&hdma_sdio_rx) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

__HAL_LINKDMA(sdHandle,hdmarx,hdma_sdio_rx);

/* SDIO_TX Init */

hdma_sdio_tx.Instance = DMA2_Stream6;

hdma_sdio_tx.Init.Channel = DMA_CHANNEL_4;

hdma_sdio_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;

hdma_sdio_tx.Init.PeriphInc = DMA_PINC_DISABLE;

hdma_sdio_tx.Init.MemInc = DMA_MINC_ENABLE;

hdma_sdio_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;

hdma_sdio_tx.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;

hdma_sdio_tx.Init.Mode = DMA_PFCTRL;

hdma_sdio_tx.Init.Priority = DMA_PRIORITY_VERY_HIGH;

hdma_sdio_tx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;

hdma_sdio_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;

hdma_sdio_tx.Init.MemBurst = DMA_MBURST_INC4;

hdma_sdio_tx.Init.PeriphBurst = DMA_PBURST_INC4;

if (HAL_DMA_Init(&hdma_sdio_tx) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

__HAL_LINKDMA(sdHandle,hdmatx,hdma_sdio_tx);

/* SDIO interrupt Init */

HAL_NVIC_SetPriority(SDIO_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(SDIO_IRQn);

/* USER CODE BEGIN SDIO_MspInit 1 */

and fatfs driver

/* USER CODE BEGIN BeforeWriteDMABlocksSection */

/* can be used to modify previous code / undefine following code / add code */

/* USER CODE END BeforeWriteDMABlocksSection */

/**

* @brief Writes block(s) to a specified address in an SD card, in DMA mode.

* @param pData: Pointer to the buffer that will contain the data to transmit

* @param WriteAddr: Address from where data is to be written

* @param NumOfBlocks: Number of SD blocks to write

* @retval SD status

*/

uint8_t BSP_SD_WriteBlocks_DMA(uint32_t *pData, uint32_t WriteAddr, uint32_t NumOfBlocks)

{

uint8_t sd_state = MSD_OK;

uint8_t *buf = (uint8_t *)pData;

uint8_t n;

uint32_t timeout = 100000;

if ((uint32_t)pData%4!=0) {

for(n=0;n<NumOfBlocks;n++){

memcpy(SDIO_DATA_BUFFER,buf,512);

/* Write block(s) in DMA transfer mode */

if (HAL_SD_WriteBlocks_DMA(&hsd, (uint8_t *)SDIO_DATA_BUFFER, WriteAddr+512*n, 1) != HAL_OK)

{

sd_state = MSD_ERROR;

}

while(SD_TxCplt == 0){

if (timeout -- == 0){

sd_state = MSD_ERROR;

break;

}

}

SD_TxCplt = 0;

buf += 512;

}

}

else {

/* Write block(s) in DMA transfer mode */

if (HAL_SD_WriteBlocks_DMA(&hsd, (uint8_t *)pData, WriteAddr, NumOfBlocks) != HAL_OK)

{

sd_state = MSD_ERROR;

}

while(SD_TxCplt == 0){

if (timeout -- == 0){

sd_state = MSD_ERROR;

break;

}

osDelay(4);

}

SD_TxCplt = 0;

}

return sd_state;

}
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Sorry, bumping old zombie unanswered threads off my feed

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..