cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f746G-disco, SD card, FatFs, f_open returns FR_NO_FILESYSTEM

koutsopo
Associate
Posted on January 29, 2016 at 12:02

Hello,

I have an application which consists of 2 threads. One thread is implementing an http client

and the other writes a file in the sd card. When i run the threads seperately they work fine,

however when I run them at the same time the f_open function returns FR_NO_FILESYSTEM.

It turns out that that is probably caused by the lwIP stack initialization function of the first thread.

I would be glad if anyone had any idea.

Thank you.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Bumping chronically old questions off my feed. @ST Community​ 

The FatFs and SDMMC code is not thread safe, you really need to serialize access to the resources. Consider having a third thread that performs all the FILE operations and services requests from the others via a state-machine.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..