Is there something else that I am missing? I have followed the instructions in UM1884 and RM0394, but after writing to BKP0R, it still reads zero (even with NoErase).0x40021058: 1006c401 1 RCC_APB1ENR1_PWREN
0x40007000: 00000300 1 PWR_CR1_DBP
0x4...
Yes, you are correct. I thought I had set the TAMP3NOERASE bit, but I was mistaken.Thank you.0x40021058: 1006c401 1 RCC_APB1ENR1_PWREN
0x40007000: 00000300 1 PWR_CR1_DBP
0x40021090: 00008200 2 RCC_BDCR_RTCSEL
0x40021090: 00008200 1 RCC_BDCR_RTC...