STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Do a corralation with DSP Library

I have a 32F746GDISCOVERY and would like to test the dsp functionalities with a correlation.I have the following code:#include "arm_math.h" extern void arm_correlate_fast_q31(q31_t * pSrcA, uint32_t srcALen, q31_t * pSrcB, uint32_t srcBLen, q31_t * p...

MMett by Associate III
  • 2082 Views
  • 2 replies
  • 0 kudos

STM32F429I-DISCO - USART3 outputs only 1.6V

Hi everyone,I am trying to get USART3 running on my STM32F429I-DISCO board. USART3 is configured with the following configurations:Mode: AsynchronousHardware Flow Control: DisableBaudrate: 115200, Word Length: 8, Stop Bits: 1GPIO: PD8 = TX, PD9 = RXI...

smrtkai by Senior
  • 2228 Views
  • 4 replies
  • 0 kudos

stm32f722ZE Nucleo UART sample code problem

Posted on January 10, 2018 at 21:56Hello, I've just built the UART sample code for the 722ze Nucleo board and have a problem. I have not modified the code (except for the transmitted character buffer).  The sample code shows setting up the unit for ...

Any STM32 in flip-chip packaging ?

Hi everyone, I was just wondering if there was any STM32 MCU in a flip chip packaging configuration ? I have seen some BGA packages but I came to understand that it didn't mean that the chip was flipped inside...Any info on the matter would be appre...

mCOZZ by Associate II
  • 2233 Views
  • 4 replies
  • 0 kudos

Exit from STOP mode

Hi everyone,I'm slightly confused here.I'm putting my micro into stop mode, but I can't seem to wake it up using an interrupt.Here's how I'm setting it:__HAL_RCC_GPIOA_CLK_ENABLE(); GPIO_InitTypeDef GPIO_InitStruct; GPIO_InitStruct.Pin = GPIO_PIN_4...

con3 by Senior
  • 1632 Views
  • 3 replies
  • 0 kudos

Resolved! Can't get a simple GPIO External Interrupt to fire

Hi there. I'm having a lot of trouble.I've managed to get UART (just direct calls, not interrupt based), PWM, and ADC working on a Nucleo board (namely, the STM32F070RB board). However, I'm having serious trouble getting a simple push-button to fire ...

0690X000006CmDsQAK.png 0690X000006CmE7QAK.png 0690X000006CmE2QAK.png
SWill.10 by Associate II
  • 1820 Views
  • 4 replies
  • 0 kudos

STM32 UART RS485 DE probelm

Hi, AllI am using STM32F303CB to build a modbus environment which connected to RS485 bus. (BTW, MCU as slave side)I using STM32 HAL lib to setup whole UART & RS485 setting. I suppose DE pin waveform should be matched to Slave_Tx ( X wrong)-> The DE p...

0690X000006Cof7QAC.png 0690X000006CofHQAS.png
clee.10 by Associate III
  • 3772 Views
  • 3 replies
  • 1 kudos

Resolved! Bugged PWM generation via timer in slave mode on STM32L496?

Hello,I implemented a simple function generator as part of a project with a NUCLEO-L496ZG-P board.A cosine signal is generated using TIM2 (internal clock, no prescaler, period set by ARR value) -> DMA (with 256 point cosine table in memory) -> DAC (t...

f.bayer by Associate II
  • 5345 Views
  • 6 replies
  • 0 kudos