STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H750 and USB3300-EZK Startup Issue

My design uses a STM32H750VBT6 MCU with the USB3300-EZK PHY for high-speed USB. The hardware and software implementations are complete and in general everything works extremely will. The only issue I am seeing is that there are occasional startup pro...

PA0-WKUP - do I have to care on INPUT?

I'm in need to scan a bunch of contacts in a 4 rows, 8 column diode matrix configuration. PA0-PA7 are the inputs, PB12-PB15 the outputs. What I'm wondering about is the PA0-WKUP special function in contrary to the rest of inputs (PA1-PA7). Do I have ...

STM32H755ZI custom board not detected by ST-Link

Hi community !I was working on a custom STM32 board as part of a robotics project. We started evaluating STM32H7 through the Nucleo boards, and now that we've confident with our chip selection, I designed a custom nucleo-type board, which can later b...

Aadi by Associate
  • 260 Views
  • 2 replies
  • 0 kudos

DFU mode for STM32N6

Hello, I'm reading the article on "How to create an STM32N6 FSBL load and run" and have a couple of questions about DFU implementation on the STM32N6: 1. Is DFU possible with the application as part of the FSBL? 2. Is there an example on how to imple...

Resolved! Per-device CAN buffer capabilities

Is there an easy way to find devices that support specific CAN buffer configurations?For example, some only have receive queues whilst others allow a number of receive buffers to be configured (which is what I want). I know the H7x7 supports this, bu...

CTapp.1 by Senior III
  • 259 Views
  • 3 replies
  • 3 kudos

ETM trace maximum data rate on STM32U575

Hello everyone,We are having trouble getting tracing to work with our target at full clock speed and would like to understand why, we have an application running on STM32U575 @ 160MHz CPU clock, we also connected the J-Tracer to it using a connector ...

Screenshot 2024-06-11 163220.jpg