STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! question aboue bootloader Write_Memory command

Hi, I am tring to write data by the FDCAN bootloader of system memory, my target is STM32H563. Now, I can read the device ID, perform the mass erase command, but I can't write data to SRAM/Flash, the FDCAN bootloader doesn't response any CAN message...

Snaku_0-1762338250957.png Snaku_1-1762338502807.png
Snaku by Associate III
  • 623 Views
  • 6 replies
  • 2 kudos

Resolved! Error in the RM0090 Rev21

Hi, I don't know where to post this message. There's an error in the RM0090 Rev21 reference manual, page 121: "bit 15 of the PWR_CR register" should be "bit 14 of the PWR_CR register". And most importantly, the debugger doesn't have bit 14 (VOS) of ...

111.png
DenMir by Associate
  • 231 Views
  • 1 replies
  • 0 kudos

Resolved! Clarification on Country of Origin for STM32H523RCT7

Hello, I hope to reach the appropriate contact regarding Country of Origin (CoO) information at ST.We have identified a conflict between the CoO listed on the website and other documents (such as PCN and the attached FMD chemical document). These doc...

MA_95 by Associate
  • 242 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H5E4/E5/F4/F5 with PLAY: boards availability?

A new STM32 sub-family (as part of the 'H5 family) came out. They have everything but the kitchen sink. As far as I can tell, 'H5E4 and 'H5E5 differ only in that the higher one has USB-HS with PHY (the 'H5Fx are crypto-enabled variants, as usually) W...

S28HS512T Issues with STM32H7S7

After encountering an issue with a Hyperbus flash chip we moved our flash to what we thought would be a simpler OctoSpi Nor Flash. I am working with an STM32H7S7 chip with a NOR Flash S28HS512T. I cannot get the chip to communicate in the desired mod...

bcompter by Associate
  • 265 Views
  • 2 replies
  • 0 kudos

STM32N6: DCMIPP

Hello,I want to use the TW9992 NTSC/PAL Video Decoder for STM32N6 to transfer an NTSC camera (720x480 resolution) to the MCU via MIPI-CSI and display it on the screen. I have attached the code below.static void MX_DCMIPP_Init(void) { /* USER CODE...

Clyasenth by Associate II
  • 4203 Views
  • 18 replies
  • 0 kudos

Resolved! Internal flash storage issue on STM32G0B1

Good day,I am writing firmware for a custom board using the STM32G0B1KET6 and am experiencing issues related to writing a serial number to the internal flash.As far as I can tell, this MCU has 512 KB of flash split into 2 banks of 128 pages (each pag...

Shaunus_0-1758113387876.png Shaunus_1-1758114807711.png
Shaunus by Associate
  • 771 Views
  • 2 replies
  • 0 kudos