STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HOW TO SAVE ADC RESULTS?

Hi everyone, I am new to the community and I am also not very expert on microcontrollers. I own a STM32F407G-DISC1. I was able to write the code for ADC (at least I think), but I don't know how to save the data on the memory. Can anyone tell me how t...

MSimo by Associate II
  • 4927 Views
  • 7 replies
  • 0 kudos

AN2606 pointing to RM0433 for STM32G43/7

Hello,AN2606 Rev 37 on page 321 writes:For more information regarding the STM32G431xx/441xx option bytes configuration, refer tohe STM32G4 reference manual (RM0433).RM0433 is the STM32H7 reference manual.

What should be the output value of ADC if input is not connected to dedicated pin? I am getting some values (230).

Hello, As I am working on analog inputs I require ADC. STM32F334 Nucleo board has 12-bit ADC (2) with 21 channels, I am using ADC1 Channel 1.After programming without applying any input to the pin (PA0) I am getting some values through USART2.Can any...

sagar by Associate II
  • 2198 Views
  • 2 replies
  • 0 kudos

Is there a simple way to prevent that the STM32F0 is supplied parasitic through the protection diodes of the GPIOs? The device seems not to provide a brownout reset circuit, or am I wrong?

We use a STM32F0 in an application with increased safety requirements. The power supply is secured by a simple fuse and we have to assure that the STM32F0 is in reset state when the fuse is blown (EN60335).Since we have a second power supply in the s...

GTelk by Associate II
  • 5215 Views
  • 13 replies
  • 0 kudos

Any ready to go Linux images for STM32F4/F7?

Hello,are there any ready to use linux images for STM32F4/F7 beside the 2.4 uCLinux image for the f4 disco from 2013? https://github.com/fdu is a good start, but I can not get uBoot to recognize the files on the SD card.

Parsing GPS Messages ???

Dear Member, I want to parse GGA,GSV,ZDA,VTG,RMC,GLL,is my container not enough ?Sometimes I can parse it sometimes I miss......?line_buffer[2048];uint8_t      rxBuffer[768];      str=strstr((char*)GPS.rxBuffer,"$GPGSV,");            ProcessNMEALine(...