STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SIM900 question ?

Dear Members,I want to test my SIM900 module,Do I need something more from this code ?printf("TEST SIM900\r\n"); //usart_pstr("AT\r\n"); target =0; //UART1 selected printf("AT/r"); HAL_UART_Receive(&huart1, (uint8_t *)&RxModem, 8,100); ...

How to combine two PWM pulses along with a delay in between?

I am using stm32756G eval board. I want to generate a pattern of two PWM pulse along with a delay. Example: A pulse of 1Khz + delay (milliseconds) + A pulse of 1KhzI am able to generate a PWM pulse of 1Khz.Is there any example for that in stm32cubef7...

phenom by Associate II
  • 956 Views
  • 2 replies
  • 0 kudos

How to program an STM32 ARM micro controller

Hi guys, I have a project where I need to use STM32 ARM processors I want to be able to program a bare chip of STM32's ARM Microcontrollers on my breadboard. I have a ST link V2 as the programmer. I would like to know what software (for free only)/ap...

Sashvat by Associate II
  • 4978 Views
  • 15 replies
  • 0 kudos

DMA to/from external SDRAM

Using the STM32F769 Disco, I've enable the external SDRAM using the FMC and can read/write that memory.I also have both SAI audio and microSD interfaces working with DMA, as long as the memory target/destination is internal SRAM. However, DMA transfe...