User Activity

Hello, at this moment i'm investigating the possibilities of our current system and would like to know if the 2 Octo-spi peripherals can be used as legacy, normal SPI.
I am using a STM32L4S9 microcontroller and used CubeMX (L4 V1.13.0 Firmware) to generate code for the USB to communicate with the device as a serial port. When sending an exact amount of bytes, 832 to be precise, the data is not send through to the P...