STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Under what conditions does bxCAN fail to transmit?

Hello, I am working on a project trying to merge 2 discrete CAN buses with the STM32F746zgt6 using bxCAN with the HAL drivers. This system will take packets in on both transceivers, one on each bus, and try to output on the opposite transceiver, esse...

ARigg by Associate
  • 671 Views
  • 0 replies
  • 0 kudos

STM32F415 - Automatic Erase of Flash on power ON

I am using Mini-M4 module with STMF415RG MCU. Module is programmed using STLink SW interface. However when the module is put on to the mother board, the flash memory gets erased when the board is powered on. What can be the reason for this automati...

MJain.7 by Associate
  • 1496 Views
  • 2 replies
  • 0 kudos

Interrupt is not work

attached my project.i generate the project using the cube.the interrupt is not workadvicethank you

ATvit by Associate
  • 755 Views
  • 0 replies
  • 0 kudos

Resolved! Interrupt duplication for AWD1 and EOS flags from ADC1

Hello.I have a Nucleo board with stm32f302r8. I want to set a state variable for voltage window:state = STATE_OK if higher threshold > current voltage >  lower thresholdstate = STATE_AWD if higher threshold < current voltage or lower threshold > curr...

KErmo by Associate
  • 1514 Views
  • 1 replies
  • 0 kudos

I want to read/write to the FLASH of STM32G071.

 I am using the Nucleo-G071RB dev board along with it's demo code. It runs fine in run mode however in debug mode I cannot see the data at the specified memory locations. I am using Keil IDE (first time user of Keil) for writing the code.. Is there a...

Pankaj by Associate
  • 3588 Views
  • 5 replies
  • 0 kudos