STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

{B-L072Z-LRWAN1:Sgfx_ModemAT] Bug about command AT$TM

If I execute "AT$TM=1,0", i obtained an error AT_ERROR.In debug, the execution of this command gave a error code 0x50 ( Device Id that should be used in SIGFOX_API_send_test_frame function must be 0xFEDCBA98 ) .I don't know why.

dramat by Associate
  • 641 Views
  • 0 replies
  • 0 kudos

have to press RESET button after programming STM32F030C8

Hi,Previously, we had a customized board based on STM32F030C6.It worked very well and it runs the main code, just after we finish loading the main flash memory, with new code (without pressing RESET key).Due to some memory constrains, we replaced STM...

STM32L151VCT6A programing

i had used STM32L151VCT6A MCU for a project i have already programmed by using st-link and tested its peripherals due to some issue on display i tried to reprogram it is not allowing to read or write it is showing an error as below attached, th...

Dgowd by Associate
  • 1355 Views
  • 1 replies
  • 0 kudos

Hi, I have an STM32L4 Discovery kit IoT node (B-L475E-IOT01A) and need to update the WiFi firmware. The firmware download relies on ST-LINK_CLI.exe and STMFlashLoader.exe so is windows only, does anyone know of a way to update the WiFi firmware on Linux?

Firmware download location: as per https://www.inventeksys.com/iwin/firmware/The uploader batch file for Windows in the download:@echo offset _ping_cmd=wmic path Win32_SerialPortfor /f "tokens=8" %%i in ('%_ping_cmd% ^| findstr /I /C:"STMicroelectron...

JDiam by Associate
  • 1194 Views
  • 1 replies
  • 0 kudos

how to interface adxl345 in stm32?

Im currently working on stm32f103r8. Now i need to interface the adx345 through SPI in stm32 also i coded for this,issue im getting here is when the simulation is running the SS is not getting low it is always in high state.please notify my mistakes...

Sm.16 by Associate II
  • 2174 Views
  • 2 replies
  • 0 kudos