STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F407 DISCOVERY board CAN example

I have tried to get the CAN peripheral up and running on STM32F407 discovery board.But I am stuck at one point. Inside method HAL_CAN_Init(CAN_HandleTypeDef *hcan), I end up in the HAL_CAN_STATE_ERROR.Is there any example available to test on the dis...

gowtham K by Associate II
  • 1547 Views
  • 2 replies
  • 0 kudos

FIT value of STM32

Hello,I need to know the FIT value of STM32F7 Series (STM32F746VGT,etc) to compute the reliability data.Could anyone tell me that information ?Thank you in advance.Toshiya

User.57 by Associate
  • 856 Views
  • 1 replies
  • 0 kudos

using 32 MHz crystall with STM32L011K4

Hi,In a project I need a precise timing so I cant rely on th internal oscilator and want to use a crystal 24-32MHz with MCU. But actually I couldnt find anything about this possibility in datasheet.the sample is 32 KHz that is not good for my applica...

MKora by Associate II
  • 1695 Views
  • 4 replies
  • 0 kudos

Why Linker file needs to be modified to use External memory(RAM/Flash) if I can access external memory using communication modes like SPI,I2C,etc ?

I have seen many examples to use external memory as heap but for it they have modified the linker and added section of needed memory. But I am curious if I can access the external memory using standard communication interfaces like I2c, SPI, etc then...

Mrunal A by Associate III
  • 1560 Views
  • 2 replies
  • 1 kudos

L4 color space clut

I only need to display around 8 colors in rgb space and if i use L4 color space i can reduce my framebuffer to the point where i can put the entire framebuffer in internal sram. The only problem is i don't understand how to format the clut in L4.

Badam.17 by Associate II
  • 1281 Views
  • 1 replies
  • 0 kudos