PSRAM with 32-bit data bus width?
According to the STM32F4/F7 data sheet FMC controller support 32-bit bus PSRAM. For my application I would like to use this configuration, due to a high bandwidth requirement. However, in the market it seems very difficult to find a PSRAM with 32-bits bus. At least I could not find anything so far. Could someone please point to some products available, if those exist?
If feasible, I could use two 16-bit PSRAM. But it was also hard to find an example of doing so. Is it possible to connect two 16-bits PSRAM to one STM32F4/F7 and write to these simultaneously?