Failed to program or debug external nor flash (h743 eval)
Hello,
Till now, I've debuged my application on internal flash with stm32h743 eval.
Now, I try to use external falsh.
But as I describe below both IAR debugging and stm32programmer fail with the external flash using the stm32cubeh7 example and the eval board.
1. I changed the following code:
-SCB->VTOR = 0x08000000
+SCB->VTOR = 0x60000000and also changed in .icf file.
But on pressing "download and debug", there is no stopping in main breakpoint. Nothing happens.
2. I then checked in IAR -> debugger -> download
The "override default .board file" was not checked, so I checked the box.
($TOOLKIT_DIR$\config\flashloader\ST\FlashSTM32H753xI.board )
Note that on checking the contents of FlashSTM32H753xI it shows 2 banks of 0x08000000 (which is the internal flash, not the external !)
Then, on pressing "download and debug" nothing happens and I don't see it stopped in main() breakpoint.
3. The next thing I tried is to use stm32programmer
I build for .out file, I then chose the correct external flash "M29W128GL_STM32H743I-EVAL", I erased the full chip , created .bin file, but on doing download it to 0x6000000 with vierfy.
Seems that erase and download is done without errors, but verification fails:
14:31:55:587 : Memory Programming ...
14:31:55:587 : Opening and parsing file: C:\projects\mcu\software\en.stm32cubeh7\STM32Cube_FW_H7_V1.3.0\Projects\proj\RHS\oper\EWARM\STM32H743_EVAL\Exe\Project.bin
14:31:55:588 : File : C:\projects\mcu\software\en.stm32cubeh7\STM32Cube_FW_H7_V1.3.0\Projects\proj\RHS\oper\EWARM\STM32H743_EVAL\Exe\Project.bin
14:31:55:588 : Size : 130031 Bytes
14:31:55:588 : Address : 0x60000000
14:31:55:588 : Erasing Segment <0> Address <0x60000000> Size <130031>Bytes
14:31:55:588 : Erasing memory corresponding to segment 0:
14:31:55:589 : Memory erase...
.....
14:31:58:219 : run ap 0
14:31:58:220 : halt ap 0
14:31:58:220 : r ap 0 reg 0 0x00000001
14:31:58:228 : r ap 0 @0x60000000 0x00000400 bytes
14:31:58:228 : Error: Verification issue at address 0x60000000 (byte = 0xFF)
14:31:58:228 : Error: Download verification failedNote that although the readme says to flash ""M29W128GL_STM32H743I-EVAL", in the EVAL guide it shows in schematic PC8F128M29EWLA.
As you can see in the log, the verification failed.
Note that erasing external full chip is successful.
Thank you,
ran