STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am new to micro-controller programming . I am using STM32F091RC Nucleo board. I am trying to read the temperature using NTC thermistor of 10 kOhm. I burned the code on micro-controller and tried to see the output on STM Studio.

 But my adc_value is stuck at 59390 for some reason. I don't see any change in temperature and I am not sure if I am doing it right. Can anyone help me?/* Private variables ---------------------------------------------------------*/ADC_HandleTypeDef ...

Pinki by Associate
  • 1747 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F30f4, standard cube configured out of the box software locks up after fixed number of processor cycles. IO looks to resets also. Loops in system memory starting at 0x1ffffed68. Only if sysTick is enabled. Does not get to sysTick interrupt.

STM32F30f4 Does this in debug mode or release with and without STLINK attached via SWCLK Pin 20,SWDIO Pin 19,NRST Pin 4.Using HSI clock and PLL , but tried also without PLL. I've only enabled IO on the standard IO lines available, PA0 -> PA7 Pin 6 to...

PKnel by Associate II
  • 2268 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H743 BDMA channel for SAI4 not described in Manual

I am trying to program BDMA of STM32H743 using Nucleo board to perform DMA Peripheral to Memory operation . What I have found a bit difficult is that I could not see any information on Reference Manual , Datasheet or on forum for the mapping informa...

A Maq by Senior
  • 1369 Views
  • 4 replies
  • 0 kudos