STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question about the LED of STM32F407

This is my code.GPIO_PinState boButton_state ;printf (" Hello �?� Cruel �?� World \n"); while (1){boButton_state = HAL_GPIO_ReadPin ( B1_GPIO_Port , B1_Pin ); HAL_GPIO_WritePin ( LD6_GPIO_Port , LD6_Pin , boButton_state );HAL_GPIO_TogglePin ( LD3_GPI...

Cl.1 by Associate II
  • 1865 Views
  • 3 replies
  • 0 kudos

Hi As a hobbyist, I am planning to make a robot that can take real-time data from the environment. I have found 2 boards on st: STM32 F411VE discovery and NUCLEO F446RE, but I don't know which one to choose.

I want to know: how many analog input pins are there in each board. which board is good at taking data from sensors continuously which would be better for USB communication with raspberry pi or is there some other boards which is good at taking analo...

MIsla.2 by Associate
  • 754 Views
  • 0 replies
  • 0 kudos

STM32 Timer Output compare

I am using STM32L476 Nucleo board and cubemx. I want to use Output compare channel 1 for timeout of 2ms. i have configure the timer but timer is not giving interrupt for Output compare. i am getting interrupt for period i gives for timer. but not for...

SS.Sagar by Associate III
  • 1621 Views
  • 2 replies
  • 0 kudos

exfat in stm32f103

Hi, All​I managed to apply sd card(SDHC, smasung evo 32gb) using sdio in cubemxAnd now, i want to apply with sd card(SDXC samsung evo 64gb) using sdio in cubemxBut some reason it didn't go well. it seems like the stm32f7 can apply exfat(in cubemx,...

Lgunh.1 by Associate
  • 1201 Views
  • 1 replies
  • 0 kudos

Resolved! How to read data as master on SPI?

I am learning serial protocols using STM32 boards (F411RE and L432KC). So far I have successfully configured the boards as master and slave to send data from one board to another, and as I checked it works perfectly(I communicate the received data fr...

0693W000000VLiLQAW.jpg
KSchr.11 by Associate II
  • 3699 Views
  • 2 replies
  • 0 kudos