Skip to main content
RSonn.706
Associate
November 1, 2019
Question

STM32F103 PC13 variable duty cycle waveform

  • November 1, 2019
  • 1 reply
  • 802 views

I'm intending to use PC13 as an output to drive the onboard LED, but at some point in my program the PC13 pin begins outputting a 4.4 khz signal with pulse width that varies from 0% to 100% back to 0% and keeps repeating that pattern at approx 4 Hz. Is this caused by the RTC calibration function? How can I turn it off. I didn't intentionally turn it on.

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
November 1, 2019

Isn't PC13 in the low-power domain? And have very low drive current

Don't enable LSE

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..