I am trying to interface a GSM sim7600 module with the STM32F446RE, but i am not getting the response on the UART.
I have checked the PIN they connected in the correct order and on the correct pins. I have checked the GSM module on hyperterminal and it is functioning as intended. I am using the HAL drivers and Kiel IDE.
I am trying to get the response from the command AT which returns
AT
OK
////////////This is for starting up the GSM module ///////////
HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_6);
HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5);
HAL_Delay(500);
HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5);
HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_6);
///////////command//////////////////////////
uint8_t at_test[]="AT\r\n";
uint8_t at_gpsinfo[]="AT+CGPSINFO\r\n";
uint8_t answer[100]="";
while (1)
{
HAL_UART_Transmit(&huart3,at_test,6,10);
HAL_Delay(500);
HAL_UART_Receive(&huart3,answer,100,100);
HAL_Delay(500);
HAL_UART_Transmit(&huart2,answer,100,100);
HAL_Delay(500);
}
both the GSM and STM32F446RE are set to 115200