STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue with freezing IWDG in stop1 mode

Hello,Issue :- STM32L4R5 controller will restarting, because of the IWDG in stop1 mode of MCU.Approach followed : As per reference manual, by clearing the IWDG_STOP bit of FLASH_OPTR register, we can freeze the IWDG counter in stop 1 mode of the MCU....

Bhushan by Associate II
  • 813 Views
  • 0 replies
  • 0 kudos

Problem with STM32F103C8T6 STANDBY mode

I am facing a realy strange problem while trying to put my stm32f103c8t6 into a standby mode. The consumption in standby mode is .8mA (what is 40 times higher then its supposed to be) on first board (Board A) and .02mA (what is 10 times higher) on se...

Markiyan by Associate II
  • 2218 Views
  • 4 replies
  • 0 kudos

STM32F745 RTC Alarm interrupt.

I have a very peculiar problem with my STM32F745 MCU. I have generated code with CubeMX which is very basic and doesn't initialize any peripherals at all. Main simply initializes the HAL, clock & then goes into an infinite loop that increments a coun...

BPetk.1 by Associate II
  • 2330 Views
  • 2 replies
  • 0 kudos

STM32 QuadSPI only BANK2

Posted on February 13, 2016 at 11:22Hello!I have the follow problem:I use STM32F745. I've chosen the QuadSPI interface for flash, to be exact, QSPI BANK2. I make initialization through CUBEMX, using HAL library. I see CLK signal only, there are no o...

shides2 by Associate II
  • 1703 Views
  • 2 replies
  • 0 kudos

Are the HSLV I/O's automatically set to work as HSLV?

I'm working with the h743 family and I'm trying to figure out how the HSLV (High speed Low voltage) I / O's work, because I don't want to use this option to avoid damaging the MCU, since my power supply is 3.3V. In more detail, I want to set FDCAN1 o...

BSant.1 by Associate II
  • 1302 Views
  • 0 replies
  • 0 kudos