Question
Supply external analog circuitry with AVDD?
So, I'm trying to integrate on a Test JIG a NUCLEO-144 with STM32F746ZG on board.
It should be possible to draw some current since AVDD (CN10 pin1) is connected through a ferrite bead to the +3.3V (and in the user manual is written that the +3.3V can be used as supply if the Nucleo is powered by VIN or E5V, the second one is my case).
So the limit of doing this should be the 500mA max of the LD39050PU33R mounted on the board.
I would need not more than 10mA, I guess.