STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I want to do file operation on internal flash memory. is there any way to do this? I tried using f_open, f_write, but its getting fail. is there any setting that we need to do?

my requirement is to do file operation. I tried it using following way.f_mkfsf_mountf_openf_write.but it cant help me. f_mkfs failed to create file system. I attached file filesystem.c for reference. please let me know any way to do this.

STura.1 by Associate II
  • 1423 Views
  • 1 replies
  • 0 kudos

STM32f429zi usart interrupts

Hi guys hope you are doing well, I am having some issues generating a USART Interrupt to receive data in my project using the Standard Peripheral Library not HAL...I wanted to ask if there is someone who might have a simple code based on usart interr...

RMang.1 by Associate
  • 1461 Views
  • 1 replies
  • 0 kudos

Peripherals not working below 3v

i try to get spi work in custom board in stm32h743VIH mcu. I'm using mco1 output clock to supply master clock to external adc converter and spi2 to read data. I want to use system with 1.8v supply voltage. I'm using stm32Cube ide to generate code. Fl...

teijo by Associate II
  • 1729 Views
  • 2 replies
  • 0 kudos

Is it possible to use HW SS with multi-slave SPI mode?

Hello,I am using DMA for one SPI slave with which requires SS Pulse mode.Now I want to use two or more slaves is it possible to use HW SS with multi slave "I think No"is it possible to use HW SS for 1st slave and SW emulated SS using GPIO for the o...

HAlzo by Senior
  • 734 Views
  • 0 replies
  • 0 kudos

STM32F303RC ADC

HI I USED STM32F303RC ADC1 ADC2 ADC3 ADC4 ONLY PROBLEM ADC 3 USED ADC3_CH1 FOR REQULAR AND CH3 FOR INJECT BOU INJECT READ IS WRONG FOR TEST CHANGE REQULAR TO CH5 AND INJECT TO CH5 AGAIN REGULAR READ CORECT BOUT INJECT READ WRONG THIS MY CONFIG ADC __...

Resolved! My ADC outputs values from 970 and above

I 'm making a voltmeter - amp meter, this one...I 'm using an STM32F030K6T6.But when nothing is connected to the input, instead of outputing 0, the ADC gives me a value around 980.VDDA is tied to VDD.Boot0 is tied to GND.These are the ADC 's settings...

GCC -flto causes linker errors for STM32L476RGT6

I have a program for which I would like to enable link-time optimization. However, once I pass the -flto flag to the compiler and linker, I get two linker errors, one complaining about multiple definition of _exit and undefined reference to _sbrk. I...

STM32L412CB (48-pin device) - USART3 RX on PB11 not working

I did set up a basic STM32_CubeIDE project with 3 USARTs.When the PB11 Pin (USART3 RX) is connected to the communication signal, the signal is corrupted to a high signal level of 2.6V and a low signal level of 1.7V. This also happens also, when I con...

KGwer.1 by Associate
  • 1081 Views
  • 1 replies
  • 0 kudos

Question about the LED of STM32F407

This is my code.GPIO_PinState boButton_state ;printf (" Hello �?� Cruel �?� World \n"); while (1){boButton_state = HAL_GPIO_ReadPin ( B1_GPIO_Port , B1_Pin ); HAL_GPIO_WritePin ( LD6_GPIO_Port , LD6_Pin , boButton_state );HAL_GPIO_TogglePin ( LD3_GPI...

Cl.1 by Associate II
  • 1822 Views
  • 3 replies
  • 0 kudos