2019-09-18 9:59 AM
Usecase:
Using the SDMMC module with DMA in HS mode (clock bypass @48MHz following CMD6 switch CMD), the SDMMC_IT_DTIMEOUT interrupt is raised when waiting few dozen of seconds after last successful data transfer (FATFS f_read in this case).
The HAL_SD_IRQHandler then calls the SD_DMARxAbort callbacks which sets the hsd->hdmatx to NULL.
Thus the following data transfer are locked as calls to HAL_SD_GetState(&sSdHdl) never return HAL_SD_STATE_READY.
Cause:
The SD_DMAReceiveCplt which is triggered before HAL_SD_IRQHandler clears the SDMMC_FLAG_DATAEND. Then the HAL_SD_IRQHandler checks for SDMMC_FLAG_DATAEND fails and the call to
__HAL_SD_DISABLE_IT(hsd, SDMMC_IT_DATAEND | SDMMC_IT_DCRCFAIL | SDMMC_IT_DTIMEOUT | SDMMC_IT_TXUNDERR | SDMMC_IT_RXOVERR);never happens, thus allowing for SDMMC_IT_DTIMEOUT to be raised even if the transfer was successful...
Fix (?) :
Change
void HAL_SD_IRQHandler(SD_HandleTypeDef* hsd)
{
uint32_t errorstate = HAL_SD_ERROR_NONE;
/* Check for SDMMC interrupt flags */
if (__HAL_SD_GET_FLAG(hsd, SDMMC_IT_DATAEND) != RESET) {
__HAL_SD_CLEAR_FLAG(hsd, SDMMC_FLAG_DATAEND);
__HAL_SD_DISABLE_IT(
hsd, SDMMC_IT_DATAEND | SDMMC_IT_DCRCFAIL | SDMMC_IT_DTIMEOUT | SDMMC_IT_TXUNDERR | SDMMC_IT_RXOVERR);
if ((hsd->Context & SD_CONTEXT_IT) != RESET) {
if (((hsd->Context & SD_CONTEXT_READ_MULTIPLE_BLOCK) != RESET)
|| ((hsd->Context & SD_CONTEXT_WRITE_MULTIPLE_BLOCK) != RESET)) {
errorstate = SDMMC_CmdStopTransfer(hsd->Instance);
if (errorstate != HAL_SD_ERROR_NONE) {
hsd->ErrorCode |= errorstate;
HAL_SD_ErrorCallback(hsd);
}
}
/* Clear all the static flags */
__HAL_SD_CLEAR_FLAG(hsd, SDMMC_STATIC_FLAGS);
hsd->State = HAL_SD_STATE_READY;
if (((hsd->Context & SD_CONTEXT_READ_SINGLE_BLOCK) != RESET)
|| ((hsd->Context & SD_CONTEXT_READ_MULTIPLE_BLOCK) != RESET)) {
HAL_SD_RxCpltCallback(hsd);
} else {
HAL_SD_TxCpltCallback(hsd);
}
} else if ((hsd->Context & SD_CONTEXT_DMA) != RESET) {
if ((hsd->Context & (SD_CONTEXT_WRITE_MULTIPLE_BLOCK | SD_CONTEXT_READ_MULTIPLE_BLOCK)) != RESET) {
errorstate = SDMMC_CmdStopTransfer(hsd->Instance);
if (errorstate != HAL_SD_ERROR_NONE) {
hsd->ErrorCode |= errorstate;
HAL_SD_ErrorCallback(hsd);
}
}
if (((hsd->Context & SD_CONTEXT_READ_SINGLE_BLOCK) == RESET)
&& ((hsd->Context & SD_CONTEXT_READ_MULTIPLE_BLOCK) == RESET)) {
/* Disable the DMA transfer for transmit request by setting the DMAEN bit
in the SD DCTRL register */
hsd->Instance->DCTRL &= (uint32_t) ~((uint32_t)SDMMC_DCTRL_DMAEN);
hsd->State = HAL_SD_STATE_READY;
HAL_SD_TxCpltCallback(hsd);
}
}
[...]
}to
void HAL_SD_IRQHandler(SD_HandleTypeDef* hsd)
{
uint32_t errorstate = HAL_SD_ERROR_NONE;
/* Check for SDMMC interrupt flags */
if (__HAL_SD_GET_FLAG(hsd, SDMMC_IT_DATAEND) != RESET) {
__HAL_SD_CLEAR_FLAG(hsd, SDMMC_FLAG_DATAEND);
__HAL_SD_DISABLE_IT(
hsd, SDMMC_IT_DATAEND | SDMMC_IT_DCRCFAIL | SDMMC_IT_DTIMEOUT | SDMMC_IT_TXUNDERR | SDMMC_IT_RXOVERR);
if ((hsd->Context & (SD_CONTEXT_IT|SD_CONTEXT_DMA)) != RESET) {
if (((hsd->Context & SD_CONTEXT_READ_MULTIPLE_BLOCK) != RESET)
|| ((hsd->Context & SD_CONTEXT_WRITE_MULTIPLE_BLOCK) != RESET)) {
errorstate = SDMMC_CmdStopTransfer(hsd->Instance);
if (errorstate != HAL_SD_ERROR_NONE) {
hsd->ErrorCode |= errorstate;
HAL_SD_ErrorCallback(hsd);
}
}
/* Clear all the static flags */
__HAL_SD_CLEAR_FLAG(hsd, SDMMC_STATIC_FLAGS);
if (((hsd->Context & SD_CONTEXT_READ_SINGLE_BLOCK) != RESET)
|| ((hsd->Context & SD_CONTEXT_READ_MULTIPLE_BLOCK) != RESET)) {
HAL_SD_RxCpltCallback(hsd);
} else {
HAL_SD_TxCpltCallback(hsd);
}
if((hsd->Context & SD_CONTEXT_DMA) != RESET){
hsd->Instance->DCTRL &= (uint32_t) ~((uint32_t)SDMMC_DCTRL_DMAEN);
}
hsd->State = HAL_SD_STATE_READY;
hsd->Context = SD_CONTEXT_NONE;
}
[...]
}and
static void SD_DMAReceiveCplt(DMA_HandleTypeDef* hdma)
{
SD_HandleTypeDef* hsd = (SD_HandleTypeDef*)(hdma->Parent);
uint32_t errorstate = HAL_SD_ERROR_NONE;
/* Send stop command in multiblock write */
if (hsd->Context == (SD_CONTEXT_READ_MULTIPLE_BLOCK | SD_CONTEXT_DMA)) {
errorstate = SDMMC_CmdStopTransfer(hsd->Instance);
if (errorstate != HAL_SD_ERROR_NONE) {
hsd->ErrorCode |= errorstate;
HAL_SD_ErrorCallback(hsd);
}
}
/* Disable the DMA transfer for transmit request by setting the DMAEN bit
in the SD DCTRL register */
hsd->Instance->DCTRL &= (uint32_t)~((uint32_t)SDMMC_DCTRL_DMAEN);
/* Clear all the static flags */
__HAL_SD_CLEAR_FLAG(hsd, SDMMC_STATIC_FLAGS);
hsd->State = HAL_SD_STATE_READY;
HAL_SD_RxCpltCallback(hsd);
}to
static void SD_DMAReceiveCplt(DMA_HandleTypeDef* hdma)
{
SD_HandleTypeDef* hsd = (SD_HandleTypeDef*)(hdma->Parent);
/* Enable DATAEND Interrupt */
__HAL_SD_ENABLE_IT(hsd, (SDMMC_IT_DATAEND));
}Can someone confirm this ?
Solved! Go to Solution.
2019-11-18 7:24 AM
Yes, confirmed (32-bit DTIMER overflow @48MHz = 90sec). The F7 SD HAL using DMA is a mess, I had to rewrite many more parts of it. Also, all the expensive calls to SDMMC_CmdStopTransfer (or even HAL_SD_GetCardState) inside interrupt do look crazy. Further, SD HAL code makes naive assumptions on execution order of the two (SD+DMA) interrupt handlers.
2019-11-18 7:24 AM
Yes, confirmed (32-bit DTIMER overflow @48MHz = 90sec). The F7 SD HAL using DMA is a mess, I had to rewrite many more parts of it. Also, all the expensive calls to SDMMC_CmdStopTransfer (or even HAL_SD_GetCardState) inside interrupt do look crazy. Further, SD HAL code makes naive assumptions on execution order of the two (SD+DMA) interrupt handlers.