STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F031K6: Storing 16-bits variable in a non-volatile memory. Which solution is preferred internal Flash / external EEPROM?

I'm using STM32F031K6 in my design. I want to store 16-bits variable (Timer's AutoReload Register) in a non-volatile memory. What is best solution for this application? Internal Flash or external 128b EEPROM ?Any STM32 example code available to store...

S.Kamath by Associate III
  • 1930 Views
  • 4 replies
  • 0 kudos

Resolved! SPI with extra CE# pulse and not enough bytes

Hey,I'm a beginner.I'm working with STM32F303RET6 and I'm trying to communicate with SST26VF064B (Flash) over SPI.This is how I configured my SPI (Using MXCuce):static void MX_SPI2_Init(void) {   /* USER CODE BEGIN SPI2_Init 0 */   /* USER CODE E...

0693W000001sUQpQAM.png
RLosc.1 by Associate II
  • 3932 Views
  • 6 replies
  • 0 kudos

STM32H750 GPIO slow compared to STM32F2 series

Driving a RGB led matrix display (HUB75E) using custom board made with STM32H750. Earlier the prototype was made with STM32F205 and there was a minute flickering in some scenarios (brightness low). so thought of designing the board with STM32H7. But ...

Raees by Associate III
  • 2440 Views
  • 3 replies
  • 0 kudos

Timer in cascade mode for PWM

I would like to control RC servos with PWM. Problem is that "Normal" PWM would waste most of the precision on the PPM period (20ms) leaving 5% of 16 or 32 bit timer for duty cycle. (1-2ms)I was reading about cascading timers and that is probably the ...

Gossamer by Associate II
  • 2828 Views
  • 5 replies
  • 0 kudos

Resolved! Query regarding the nuances of encoder mode

Hi, I have an incremental encoder with 2400 counts per rev that is connected to a ball screw with a pitch of 5mm. I'm trying to accumulate the total count which I then use to calculate the exact distance of the object attached to the ballscrew. I've ...

H745ZI-Q unable to load a different program then demo

Hi,recently I switched from Arduino to Nucleo and now I wanted to play around with the H745ZI-Q and was following the step by step guide by st. Whenever I try to load a program to the mcu, only the demo blinky program is running. I have not found any...

NUCLEO board/ST-Link not detected on Windows 10 laptop

Hi all, I'm having a trouble programming my F303K8 board on my Windows 10 laptop. It will power on (LD2), but it will not connect to the computer (LD1 blinking slow red). The laptop does not detect any device being plugged or unplugged, there is noth...

JBegu.1 by Associate
  • 1568 Views
  • 0 replies
  • 1 kudos