STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Question on STO_ acronym in ST code

In trying to understand some motor control code in the ST Library I've come across some procedure names with STO_ as a prefix. Simple question what does the acronym STO mean?

BTrem.1 by Senior II
  • 991 Views
  • 1 replies
  • 0 kudos

Having Trouble with SD DMA on STM32L452 MCU

Hello. So like title says I am having trouble making SDMMC work with DMA in 4 bit mode. I tried with FreeRTOS and without FreeRTOS didnt get anyresult. But it works perfectly without DMAIt gives either Rx Overrun error or timeout error. I tried it wi...

KKurt.1 by Associate II
  • 981 Views
  • 1 replies
  • 2 kudos

Resolved! STM32L073CZ in full production?

We are intending to design in this MCU. Does ST have a website that would indicate where this part is in its lifespan? I can only see that it is listed as "active".Thanks

RSoen.1 by Associate III
  • 1014 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F091CCT6: Why my led doesn't blink?

Hi there.I have a board from some equipament which has a STM32F091CCT6 uC, and there are 3 leds, connected to pin GPIO_C13, GPIO_C14 and GPIO_A7. Anode from leds are connected to Vcc and Catode are connected in a resistor and then to the uC pins (so ...

Rick1 by Associate II
  • 1529 Views
  • 3 replies
  • 0 kudos

Need help to blink LED with STM32F2

Hello all i am trying to implement a simple thing that is trying to blink LED using a function. Below attached are main.c, project.c and project.h. If i try the same thing without using a function it works fine but if i use the function it doesnot bl...

NSirm.1 by Associate III
  • 2923 Views
  • 2 replies
  • 0 kudos

STM32H743II spi master half duplex tx into rx

spi half duplex with dma,change tx ino rx,when finished tx process,start rx process,just set the "spe" bit of spi master(not set cstart bit),dma just starts working,and cntdr goes to zero,then rx process fail,spi report overun error.

Wdong.2 by Associate
  • 945 Views
  • 1 replies
  • 0 kudos

Is "passive" participation possible?

Unfortunately I got a message that I may not attend to the workshop.I'm not interested in getting a Disco-Board for free - I can buy it by myself.Is it possible to particitpate the workshop as a "passive" member?I need no possibility to ask questions...

Sven1 by Associate II
  • 1318 Views
  • 2 replies
  • 0 kudos

Is passive participation possible ?

Hello, I have also just received a message saying I cannot attend. I do not need to get the free board (which I can by myself), Is it still possible to attend ? Thanks and best regards. Sara

SGras.11 by Associate
  • 914 Views
  • 1 replies
  • 0 kudos