STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STMCUBEIDE - STM32L010 ROM(Flash) size exceeding

I am using STMCUBEIDE there i was using optimization level as "optimize for debug". there i used a local variable as uint8_t and i am incrementing its counts then memory exceeded to 85%. if i removed increment then only 37% flash memory occupied.

Peripheral current/power consumption data for STM32L476RG

Dear community,I am planning on using the STM32L476RG for a project. That project is a low power application, so the current consumption is really important to this project. However I cannot find any reliable source for the current consumption of the...

AHass.1 by Associate II
  • 1769 Views
  • 2 replies
  • 0 kudos

directly read register status instead of HAL_GPIO_Readpin();

i am trying to bit bang 14 bits grey code. my output is not steadyuint16_t readbits(uint16_t dataPin, uint16_t clockPin) { uint16_t value =0;  for (int i = 0; i <14; ++i) {   value <<= 1;  HAL_GPIO_WritePin(GPIOC, clockPin, GPIO_PIN_RESET);  delay_...

YTimm.1 by Associate II
  • 4942 Views
  • 12 replies
  • 0 kudos

BRR of STM32F401RCT6 changed when hot swapping

When the USART is  hot swapping,some datas will occur on TX RX pin;and the value of BRR register will be changed;the picture 1 shows the BRR before  hot swapping;and the picture 2 shows the BRR after  hot swapping. Why this question happens?And what...

Pzhu.1 by Associate II
  • 1663 Views
  • 2 replies
  • 0 kudos

SPI1_NSS conflicts with PA15 in STM32F103

Hi,According to datasheet, The main function of PA15 is JTDI, so I disabled JTAG and config that pin in AF_PP mode.Then if I don't initialize SPI1, I can control PA15 as GPIO. But if I initialize SPI1, this pin will hold high. Since SPI1 has occupied...

Sni.1 by Associate
  • 2304 Views
  • 2 replies
  • 0 kudos

Resolved! Question on STO_ acronym in ST code

In trying to understand some motor control code in the ST Library I've come across some procedure names with STO_ as a prefix. Simple question what does the acronym STO mean?

BTrem.1 by Senior II
  • 992 Views
  • 1 replies
  • 0 kudos

Having Trouble with SD DMA on STM32L452 MCU

Hello. So like title says I am having trouble making SDMMC work with DMA in 4 bit mode. I tried with FreeRTOS and without FreeRTOS didnt get anyresult. But it works perfectly without DMAIt gives either Rx Overrun error or timeout error. I tried it wi...

KKurt.1 by Associate II
  • 981 Views
  • 1 replies
  • 2 kudos