cancel
Showing results for 
Search instead for 
Did you mean: 

TIM1 Chan1 PWM, no output, GPIO works fine

Davorin
Senior

Good afternoon

Configured TIM1 of a F070CBT6 to drive 3 PWM channels on PA8/PA) and PA10....

PA9 and PA10 work fine..only for channel 1 I don't see any output..furthermore it seems to be floating as when touching with a finger the attached 7406 driver turns the LED on...

OTOH when using PA8 as a general GPIO output, it works just fine to turn LED on/off...

Timer1 channel 1 output broken?

static void MX_TIM1_Init(void)
{
 
  /* USER CODE BEGIN TIM1_Init 0 */
 
  /* USER CODE END TIM1_Init 0 */
 
  TIM_ClockConfigTypeDef sClockSourceConfig = {0};
  TIM_MasterConfigTypeDef sMasterConfig = {0};
  TIM_OC_InitTypeDef sConfigOC = {0};
  TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
 
  /* USER CODE BEGIN TIM1_Init 1 */
 
  /* USER CODE END TIM1_Init 1 */
  htim1.Instance = TIM1;
  htim1.Init.Prescaler = 48000-1;
  htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim1.Init.Period = 1000-1;
  htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim1.Init.RepetitionCounter = 0;
  htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
  if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
  {
    Error_Handler();
  }
  sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
  if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
  {
    Error_Handler();
  }
  sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
  if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
  {
    Error_Handler();
  }
  sConfigOC.OCMode = TIM_OCMODE_PWM1;
  sConfigOC.Pulse = 0;
  sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
  sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
  sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
  sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
  sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
  if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
  {
    Error_Handler();
  }
  sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
  sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
  sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
  sBreakDeadTimeConfig.DeadTime = 0;
  sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
  sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
  sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
  if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN TIM1_Init 2 */
 
  /* USER CODE END TIM1_Init 2 */
  HAL_TIM_MspPostInit(&htim1);
 
}

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
TDK
Super User

Check HAL_TIM_MspPostInit() to ensure pins are initialized as AF correctly.

Failing that, look at GPIO registers to see how PA8 is configured.

If you feel a post has answered your question, please click "Accept as Solution".

Hmm..okay....

Just discovered that TIM1 channel 2 and channel 3 also behave differently when freshly programmed via J-Link or after a power-up...

After programming it seems that the counter value set is inverted...(short dark LED phase) where as after reset I see short LED on pulses as it should be...

Didn't had this on the Nucleo-F070 board...

waclawek.jan
Super User

Set PA8 as GPIO Out and wiggle - works? (aiming at bad solder joint).

Read our and check/post the relevant GPIO and TIM registers content.

JW

Yes...pin toggling works as mentioned before...

Also in pwm mode when I set a pull-down...the output isn't floating anymore...so LED doesn't light up when touching the PA8 pin...

Gotta check tomorrow more..already late here in \.ch (o;

TDK
Super User

> Also in pwm mode when I set a pull-down...the output isn't floating anymore

In PWM output mode, the pin is either set to low or high. A pulldown shouldn't be affecting it.

Edit: unless maybe it's floating during the break dead time? Not sure, but I doubt it.

If you feel a post has answered your question, please click "Accept as Solution".