STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0 Minimum EXTI Pulse Width

Hi Folks,I'm working with an STM32G0B1MCT6. In my application I need to be able to react to pulses with a width of about 5 ns. It seems the only way I could pull this off is with the rising edge detection in the EXTI controller, or some additional ex...

gdbeatl by Associate
  • 1254 Views
  • 4 replies
  • 3 kudos

Resolved! I2C Bootloader Slave address

Hi,I’m working on the STM32G491 series. In my current project, the STM32 is configured as an I2C slave and communicates with another processor over I2C.When entering bootloader mode for flashing, the STM32 responds with the slave address 0x5F, which ...

abhijith_raj_0-1750410440146.png

Resolved! Can I2C pins be in different ports?

Hi,I’m currently implementing I2C in slave mode using the STM32G491 series. Due to pin constraints, we’re considering using SCL and SDA pins from different GPIO ports—for example, SCL from port PA and SDA from port PC. Is it acceptable to assign I2C ...

Resolved! Possible risks of voltage drop in VDD of STM32F3

Hi !I am evaluating the risks associated with STM32F3, where I am speculating a case where the voltage drops in VDD for few microseconds. For an example, let us assume the voltage drops from 3.3V to 3.0V for few microseconds. This occurs every x ms (...

mechatron by Associate III
  • 924 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H750 rev V or Y

Hello ST experts,I have bought a STM32H750IBT microcontroller. Could you please let me know how I can find whether it is V revision or Y revision device?

STM32F103C8T6 Incorrect Memory Size

Recently i bought this STM32F103C8T6 Board along with ST Link V2 I was trying to upload a HEX(60KB) file using STlink software but i noticed something wierd, memory size in both pics is showing 256KB but this device only comes with 64KB flash memory ...

STM32F103C8T6.png Screenshot 2025-06-19 123755.png Screenshot 2025-06-19 123829.png
Titan by Associate II
  • 3208 Views
  • 11 replies
  • 1 kudos