STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What to do with unused IO's

Here in the below image from the Cube MX it suggests that, SET all the free pins as analog (to optimize the power consumption). How does it help. Also is it applicable to all the controller families?  

DJ1_0-1698466663322.png
DJ1 by Associate III
  • 3195 Views
  • 6 replies
  • 1 kudos

External resistor for my oscillator design

Hi, I have a question about this highlighted text in the AN2867 document refering to the "calculating external resistor" paragraph As I understood the condition to use a Rexternal is "if the power disipated in the crystal is higher than the value spe...

Aldo_Flores_Aguayo_0-1750110581049.png

SPI Communication with AD5592 ADC/DAC

Hello, I'm attempting to work with the AD5592 ADC/DAC in SPI mode and am unable to confirm communication. I'm attempting to read and write to single registers to determine whether communication takes place since I don't have an oscilloscope or logic ...

Avid_0-1750570514141.png Avid_1-1750570786858.png Avid_2-1750570825761.png Avid_3-1750570852835.png
Avid by Associate III
  • 948 Views
  • 1 replies
  • 0 kudos

Resolved! Can I use OCTOSPI as a Classic SPI?

Hi. I am using STM32H735VG for SPI communication with external ADCs.But I want to add external ADCs and I already used all 5 SPIs.So I will use OCTOSPI, can OCTOSPI play the same role as classic SPI?In menual, OCTOSPI in indirect operating mode works...

giwonKIM by Associate III
  • 4449 Views
  • 6 replies
  • 1 kudos