STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L412CBT6P startup problem

I have soldered MCU chip to a PCB and programed it by ST-Link using STM IDE.when I run MCU using ST-Link it is working fine. But When I use an external DC supply it's showing malfunction, (most of the time not working). I have connected the BOOT0 pin...

Spatr.1 by Associate
  • 886 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F745 FMC SDRAM Interface Theoretical Timining

Hello,I want to setup a STM32F745IEK6 together with an SDRAM from Micron Type MT48LC8M16A2P-6A.I analyzed the theoretical signal Intergrity for the devices and I had to end because of my question:The setup time of MT48L is required with min. 1,5 ns. ...

FGrie.1 by Associate
  • 1185 Views
  • 1 replies
  • 0 kudos

SYSCLOCK configuration problem on STM32F100VE

Hello, I have a software that has been workingfine for several years on a STM32F100VCT6. However, today we are trying to use thissoftware on the MCUs ref: 100VDT6 or 100VET6. On these 2 new references no programming problem with the same binary file....

VCedr.1 by Associate
  • 1697 Views
  • 2 replies
  • 0 kudos

Resolved! Volatile qualifier does not matter in my interrupt routine

I am new to embedded C, and I recently watched some videos about volatile qualifier. They all mention about the same things. The scenarios for the use of a volatile qualifier :1. when reading or writing a variable in ISR (interrupt service routine)2....

MJoe.1 by Associate II
  • 3278 Views
  • 5 replies
  • 0 kudos

STM32F429 Flash write/read

I'm trying to write and read some data into flash. But not work. Anybody help me?I'm using Cubeide and STM32F429 board.char test_data[]="TEST";char test_data2[5];uint32_t PAGEError = 0; FLASH_EraseInitTypeDef EraseInitStruct; EraseInitStruct.TypeEras...

ECARV.1 by Associate
  • 1640 Views
  • 1 replies
  • 0 kudos

FDCAN - multiple frames sent from single send request

Hello,I'm beginning to bring up a PCB which is based on the STM32G484QET. Initially, I'm getting the FDCAN set up (although I'll be using it as a CAN 2.0 node). I am using FDCAN1.I'm at the stage that I can transmit CAN messages which are picked up c...

NElli.2 by Associate
  • 1124 Views
  • 0 replies
  • 0 kudos

Counting up from GPIO READ

Hi,all:I wrote a code for counting up when GPIO ReadPin change high level to low, here is the code:while(1){ HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, GPIO_PIN_SET);​ if(HAL_GPIO_ReadPin(GPIOE,GPIO_PIN_10)==1) { HAL_Delay(1); if(HAL_GPIO_ReadPin(GPIOE,GP...

CGran.2 by Associate II
  • 3275 Views
  • 4 replies
  • 0 kudos