2021-02-19 7:23 AM
How can i modify this part of code to can send the register address of 16 bits
/* Implementation of I2C read for 16-bit values */
int32_t mlx90632_i2c_read(uint16_t Reg, uint16_t *value)
{
uint8_t data[2];
int32_t ret;
ret = I2C_TxRx1(MLX_I2C_Adress,&Reg, data, sizeof(data));
//Endianness
*value = data[1]|(data[0]<<8);
return ret;
}this is the I2C_TxRx1 funcion function
/* Only for MLX90632 Temperature Sensor */
ADI_HAL_STATUS_t I2C_TxRx1(uint32_t address,uint16_t *regAddr, uint8_t *anRxData, uint8_t size)
{
if (adi_i2c_SetSlaveAddress(i2CDevice, address)) // bottom-end
{
//DEBUG_MESSAGE("couldn't set slave device address");
}
tran.pPrologue=regAddr; /*!< Prologue pointer. */
tran.nPrologueSize=2;; /*!< Prologue byte count. */
tran.pData=anRxData; /*!< Data pointer. */
tran.nDataSize=size; /*!< Data byte count. */
tran.bReadNotWrite=true; /*!< Read/write flag. */
tran.bRepeatStart=true; /*!< Repeat start flag. */
ADI_HAL_STATUS_t ret=0;
uint32_t hwErrors;
adi_i2c_ReadWrite(i2CDevice,&tran,&hwErrors);
return ret;
}And this the i2C DEVICE Command/Data Transaction Structure
*****************************************************************************/
typedef struct {
uint8_t *pPrologue; /*!< Prologue pointer. */
uint16_t nPrologueSize; /*!< Prologue byte count. */
uint8_t *pData; /*!< Data pointer. */
uint16_t nDataSize; /*!< Data byte count. */
bool bReadNotWrite; /*!< Read/write flag. */
bool bRepeatStart; /*!< Repeat start flag. */
} ADI_I2C_TRANSACTION;