User Activity

Hello,I am facing a glitch issue when the frame buffer is switching with a custom widget. Both frame buffer seems to be initialized when screen enter. A few part of the area is redraw on one framebuffer. Then I have a few update on the second framebu...
I am facing performance issue due probably to my way for invalidation on data update. I have widget inside container that are not visible. When I have a data change, I update the content of the widget and invalidate the textarea for example. But this...
Hello,I just try the latest 4.19.1 (coming from 4.18.1) and the performance of this new release is just horrible in my project. Regarding the release note, I do not see anything that can really explain a slowest behaviour as it seems most of the upgr...
I am using Touchgfx 4.13.0 in my application for a while and decide to upgrade to 4.17.0 (about time you can say). But it seems that the font management evolved, and as my product is upgradable OTA, I cannot really afford to resend all fonts in bluet...
After the validation of my CM4 application in the dual core I wanted to find a way to launch it automatically on power ON, which was not the case. The CM7 was running a touchgfx application, which was stopped during my debug session on CM4. Trying to...
Kudos from