STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem with outputting LSE clock on PA8 pin as MCO

Hi!I'm trying to output the LSE clock on the PA8 pin on my Nucleo64 STM32L476 board.The code I have written is the following:#include<stdint.h>   #define RCC_BASE_ADDR 0x40021000UL   #define RCC_CFGR_REG_OFFSET 0x08UL   #define RC...

eidetech by Associate II
  • 3475 Views
  • 7 replies
  • 0 kudos

Resolved! How to generate hex file in STM32H750vb?

I am trying to generate hex file for my boot loader. I need a fix length hex file for my boot loader. I tried arm-none-eabi-objcopy -O srec --srec-len 0x10 ${ProjName}.elf ${ProjName}.srec;arm-none-eabi-objcopy -I srec -O ihex ${ProjName}.srec ${Proj...

JP_RS by Associate II
  • 1612 Views
  • 1 replies
  • 0 kudos

Does the RTC run when Vdd = 0 but Vbat = 3 volt?

I have a STM32F373VBTx serie. I know that the RTC saves the backup registers for every second. But when I restart my STM32, then the RTC sets to default date and time again due to the MX_RTC_INIT() function who is generated by CubeMX.I have two quest...

DMårt by Lead
  • 900 Views
  • 2 replies
  • 0 kudos

STM32 interrupt pin strange behavior

I am using stm32cubeide to program a stm32f030f4p6 MC. I have assigned one pin as an external interrupt and it is connected to the data output of an RF433 receiver. Here is a summary of my code:int k;   int main(void)   {   while (1)   {   k=0;   ...

0693W00000DnW4UQAV.png

Resolved! STM32F413 ADC DMA AnalogWatchdog not working in SleepMode

The goal is to have the microcontroller which is in sleep mode, wake up when the voltage on a certain ADC channel drop below a set voltage.The plan was to put the core to sleep via HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON, PWR_SLEEPENTRY_WFI)...

Pain by Associate II
  • 1797 Views
  • 2 replies
  • 0 kudos

N25Q128A13EF840F External Flash read write example

Hi,I am new to QSPI. I working with stm32f469 disco that comes with external flash N25Q128A13EF840F. I had done the GUI part now I need to store data to external flash but I don't know how to do it. I had initialized qspi with STMCUBE default initial...

himsha by Associate II
  • 2114 Views
  • 2 replies
  • 0 kudos