cancel
Showing results for 
Search instead for 
Did you mean: 

Can STM32G030Kx (LQFP32 package) high speed external clock signal (HSE) be generated from external crystal resonator, or it can be generated from external clock generator ONLY?

VRusi
Associate

In STM32G030x6/x8 datasheet (DS12991 Rev 3, Table 12 on page 31) I see only input pin for external HSE clock source (LQFP32, pin 2 - PC14 - OSC_IN), but don't see OSC_OUT pin of HSE OSC.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

It doesn't have an OSC_OUT pin, so it needs an external clock source for HSE and can only run in bypass mode.

If you feel a post has answered your question, please click "Accept as Solution".
VRusi
Associate

Thanks for your reply. It is a pity, that the documentation does not explicitly state that the HS OSC of the STM32G030 MCUs in the TSSOP20 and LQFP32 packages can only work from an external clock generator.